Associate III
Jul 10, 2024 2:48 PM UTC
Solved
STWBC86 Overheating
- 14 replies
- 4921 views
Hello,
I've designed a PCB with a schematic nearly identical to the STEVAL-WBC86TX. The only modifications are a capacitor and coil size change, which I've also implemented on a development board for direct comparison.
On the development board, my receiver PCB performs almost flawlessly, with the only issue being a charging current of around 60mA (which may be unrelated). However, on my new transmitter board, it almost immediately overheats and shuts down.
I've attached an image from WPSTUDIO showing the temperature reaching 100°C before shutting down and repeating this cycle.
Can anyone suggest potential causes for this issue or point me in the right direction for troubleshooting?
Thank you, Mike