Skip to main content
Associate II
May 2, 2025
Solved

STWBC86 operating frequency

Does the charger IC ever operate outside of the specified TX FREQ MAX and TX FREQ MIN limits?

For example, if the limits are set to 100kHz and 148kHz and the charger is operating at either limit, would FSK cause it to change the frequency below this value? If so, how much would the frequency be exceeded?

This topic has been closed for replies.
Didier HERROUIN
Didier HERROUINBest answer
ST Technical Moderator
May 5, 2025

Hello,

The FSK signal is used by the charger to communicate to the Receiver during the identification phase mainly, and it is superimposed to the power signal. It does not impact the operating frequency range which is defined by NVM parameters in the charger.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Didier HERROUIN
Didier HERROUINBest answer
ST Technical Moderator
May 5, 2025

Hello,

The FSK signal is used by the charger to communicate to the Receiver during the identification phase mainly, and it is superimposed to the power signal. It does not impact the operating frequency range which is defined by NVM parameters in the charger.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.