Skip to main content
JAKE2
Associate III
Mar 16, 2023 6:44 AM UTC
Solved

STWBC86-> Is it okay to connect the 'VINV' and VIN' with a USB +5V power supply?

Wating for your response..

Sincerely yours, Jake Kang.

Edited) It is because the datasheet said that VINV is for INVERTER INPUT. If anyone have an idea, please keep me in the loop.

    This topic has been closed for replies.
    EAYDIN
    EAYDINBest answer
    Visitor II
    Mar 20, 2023 5:52 AM UTC

    In the datasheet, it says their voltage range are from -0.7V to 27V, which covers even USB-C protocol. In addition, in pin function description, it says for both that they are power supply inputs. Therefore in my opinion, you can connect them with a +5V USB supply but don't forget to put filtering capacitors as they contain too much AC noise.

    2 replies

    EAYDIN
    EAYDINBest answer
    Visitor II
    Mar 20, 2023 5:52 AM UTC

    In the datasheet, it says their voltage range are from -0.7V to 27V, which covers even USB-C protocol. In addition, in pin function description, it says for both that they are power supply inputs. Therefore in my opinion, you can connect them with a +5V USB supply but don't forget to put filtering capacitors as they contain too much AC noise.

    JAKE2
    JAKE2Author
    Associate III
    Mar 21, 2023 4:21 AM UTC

    I put one 100nF, three 10uF capacitors between USB Input (VBUS) and GND in parallel, and connected VINV and with VBUS. I will figure it out as I experiment, thanks for your reply !