Skip to main content
Associate
October 7, 2024
Question

STWBC86 aplication

Hello,

I am currently working on the implementation of the STWBC86 chip, following the STEVAL-WBC86TX as a guide. If we want to develop a PCB with the STWBC86 chip, is it possible to load the initial configuration by connecting the PCB via I2C with a USB converter to the computer? Or is external hardware, such as the STM32 development board, required to load the configuration onto our PCB?

Thank you in advance for your attention.

This topic has been closed for replies.

3 replies

ST Technical Moderator
October 9, 2024
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DEIQOAuthor
Associate
October 11, 2024

Thanks for responding.

Yes, it turns out that what we want is to replicate the STEVAL-WBC86TX and just remove some things from it, but we see that it comes with a configuration using the FT260Q chip that would be the U3 (in the image), which they use for I2C Communication, converting it to USB- C and from there to the PC. I would like to know if with this same STEVAL chip we can upload the initial configuration of the new board.I2C.png

ST Technical Moderator
October 11, 2024

yes 

it is same with STEVAL-USBI2CFT Dongle chip

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.