Skip to main content
JAKE2
Associate III
Dec 24, 2024 5:11 AM UTC
Solved

STWBC86 and STWLC38 Adaptive Charging Circuit

Hi,

We are currently testing the above chips.

I have a few questions:

  1. Can I get information or documents stating how to download firmware using an external MCU and the reference design for that? We use 3.3V I2C communication, and I understand the ST chip uses 1.8V.

  2. When I connect an MCU to the ST wireless charging chip, can I manually control the register to manipulate the total current? For example, by calculating the RX side's thermal condition and changing the TX DC MAX/TX DC PING registers in real-time when the chip gets hot to lower the temperature. Our design sometimes gets hot, causing the charging to turn on and off.

  3. If number 2 is possible, should I connect the MCU to both TX and RX, or just one?

 

My question might not be very clear, so I am willing to accept an answer that is close enough. I would appreciate your response.


This topic has been closed for replies.
JAKE2
JAKE2Best answer
Associate III
Dec 24, 2024 7:09 AM UTC

 

Because I have already completed FTP programming through the GUI.

I would like to know if I can control the registers, shown in black text on the GUI, using an external MCU and I2C communication?

 

26th - 12 - 24Edited)
Oh I found it, thanks.

https://github.com/STMicroelectronics/STWirelessCharging-C-Drivers

1 reply

JAKE2
JAKE2AuthorBest answer
Associate III
Dec 24, 2024 7:09 AM UTC

 

Because I have already completed FTP programming through the GUI.

I would like to know if I can control the registers, shown in black text on the GUI, using an external MCU and I2C communication?

 

26th - 12 - 24Edited)
Oh I found it, thanks.

https://github.com/STMicroelectronics/STWirelessCharging-C-Drivers