Skip to main content
Associate II
August 20, 2024
Question

STWBC2-HP Evalobard

Hi All,

I have developed my own Evalboard for the STWBC2-HP based on the STEVAL-WBC2TX50. Now i have flashed the stdes-50w2cwbc_FW_v1.0.0.0.hex firmware to the board and the Software shows the following. The power transfer does not work. Do you have any suggestions why that is so?

 

Thank You

 

simonh_0-1724138049367.png

 

This topic has been closed for replies.

5 replies

ST Technical Moderator
August 20, 2024

Hi Simon

i think you use wrong hex file, correct version is 1.3.0.0, please use this attach file.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
simonhAuthor
Associate II
August 20, 2024

Ok thank you. 

But with this hex file loaded, it is nearly impossible to connect to the IC via UART. The most time this error occurs when connecting:

simonh_0-1724139600881.png

 

Is it possible to initate the Calibration via SWD interface with the STM32 Cubeprogrammer?

 

After a few times trying to connect it worked, but now i get the following message: SCHEDULER-MSG-ERROR

The error log is attached.

 

ST Technical Moderator
August 20, 2024

Hi

 

Please erase all and download again, i have retest and do not have connect issues.

willzhou_1-1724140466150.png

 

 

willzhou_0-1724140443700.png

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
June 7, 2025

Hi there,

I saw your post about flashing your device with the stdes-50w2cwbc_FW_v1.0.0.0.hex firmware. I'm looking for the same firmware myself. Could you please let me know where you found it? If you happen to have a backup, would you be willing to share a copy with me?

Thanks a lot!