Welcome @gregelectric, to the community!
Register 0x10 is the register TYPEC_MONITORING_STATUS_1, whose bits have the following meaning (see the register file e.g. here:(
- [3] VBUS_READY
- 0: VBUS disconnected (Unpowered or vSafe0V)
- 1: VBUS connected (vSafe5V or negotiated power level)
- [2] VBUS_VSAFE0V
- 0: VBUS is higher than 0.8V
- 1: VBUS is lower than 0.8V
- [1] VBUS_VALID
- 0: VBUS is lower than 3.9V
- 1: VBUS is higher than 3.9V
- [0] VCONN_VALID
- 0: VCONN is lower than 4.1V or 2.7V
- 1: VCONN is higher than 4.1V or 2.7V
If your check (vbusStatus & (1 << bit_x)) returns true, that bit at position x must be set. This in turn is to be interpreted according to the register table as VCONN > 4.1V/2.7V (bit 0) or VBUS > 3.9V (bit 1).
Hope that helps?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.