STUSB4710(A) doesn't output power
- 2 replies
- 2819 views
Dear Team,
I recently created a custom PCB where I wanted to implement the STUSB4710(A) for charging a phone and other accessories. The STUSB4710 should be plug and play without the need of configuring the PDO because it is already selected. I based my design on the valuation board of this IC: STEVAL-ISC004V1. I will attach a file with my schematics.
So when I attach my Samsung A53 it will say that is is attached to a fast charger but when I look at the ampere app I charge with a current of 200mA which is almost nothing.
So I started measuring and encountered an issue where the VBUS has a stable 5V which is good, but there isn't any current running from the to the usb-c connector as I also saw in the app. I read some registers trying to find out what the problem is via I²C and read the register of the CC_STATUS (0x11h) I found this in the file that was posted in a other post. here I can see that I get the following value 0x89 which means: (0x80) twisted cc2 lines (OK), (0x09) 01001: (ATTACHWAIT_SRC) (NOK). SO next on I connected my Logic Analyzer to the CC lines for trying to see what is happening in this communication. Here he tries 2 times a reset I think but I have no idea what it could mean:
and then again after half a second approximately: 
Is there somewhere a document for understanding the communications between the cc lines?
Or do I have to send a command to a register of the sutsb4710 to start the charging?
If you need more info feel free to ask.
Thanks for the support,
Matthias H