Skip to main content
Visitor II
February 8, 2024
Question

STUSB4700 application without I2C conifuration

What happens if I use STUSB4700 in my application but I do not communicate with the STUSB4700 over I2C? Will the STUSB4700 negotiate a contract as a source with the sinking device and offer the PS FB voltages which are connected to the GPIO? I would like to provide a maximum of 15V by leaving GPIO3 and GPIO4 open circuit and negotiate a 3A maximum to the source which I believe is the NVM so I should have to communicate over I2C. I would like an automotive grade part but maybe the STUSB4710 would be the only solution for me?

This topic has been closed for replies.

2 replies

Visitor II
March 13, 2024

As is explained in the datasheet, there is a default configuration for example, for stusb4700:

RogerMun_0-1710341648765.png

If you leave GPIOs open circuit, the IC will negotiate some PDOs but won't be capable of setting the desired voltage, so the Vbus_en_src will open the switches and you won't have any output. So, in conclusion, you won't be able to charge any device which is capable of being charged at the PDOs that you are leaving open circuit.

If 15V 3A is ok for your application, i would recommend you to make a design capable of delivering all the default PDOs stored in the IC NVM.

Associate II
July 31, 2024

I have a PD Powerbank which can handle alot of PDO's

How would i connect this to the STUSB4700 for a 12V 3A factory configuration (since i dont have the option for software programming)


How would i do this?