Skip to main content
Associate
June 7, 2024
Question

STUSB4500 Default PDOs without I2C

Hi, 

We like to use the STUSB4500 without having it to progamm via the I2C. So we need to use the standard configuration. If I understand well, these are has 3 PDOs: 5v/1.5A - 15V/1.5A and 20V/1A.

However, the 20V/1A is too high. Is there a way to prevent the 20V/1A. and to only have the two PDOs  5v/1.5A - 15V/1.5A active. (without to programm the I2C)

Thanks,

Olaf

This topic has been closed for replies.

2 replies

ST Technical Moderator
June 7, 2024

HI

Please refer to DS page 25, some pin can set as your requirement.

willzhou_0-1717764337665.png

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
OlafMAuthor
Associate
June 7, 2024

Hi,

Indeed the 5V, 9V and 12 V output would be great. Looking at the table, I see SNK_PDO_Numb =3 and Power_only_Above5V =0. However, I do not understand, how and which pins I need to use to configure? Can you explain?

Thanks