Skip to main content
Associate
October 10, 2024
Question

STSPIN958 Thermal shutdown does not work

Hi,

We are using STSPIN958 for BLDC control, and under 33V, 2A, when external force applies to servo, and the current goes up to about 2A, the chip burns before the thermal shut down kicks in.

I would also like to know the value of "Tsd" delay timing parameter in thermal shutdown sequence: Figure 16 of page 21/34 of its datasheet. This value is not published.

Thanks,

Amin

3 replies

Cristiana SCARAMEL
ST Employee
November 12, 2024

Hello @amin.kamal  and welcome to the ST Community.

For a better support, could you share more details about your application?
- What configuration is the STSPIN958 working in?
- What kind of control are you applying?
- How are you measuring the motor current?

I suggest to monitor the LSSx and OUTx pins to check if any voltage overshoot occurs on these pins.

Concerning the intervention time of the thermal shutdown protection, it is few tens of microseconds.

"If you feel a post has answered your question, please click ""Accept as Solution"""
Associate
November 12, 2024

It is BLDC application.

Two STSPIN958 chips are being set in Dual Half Bridge PWM Trimming mode, and 3 lines of motor outputs are connected to BLDC.

A PID position control is applied from the servo encoder to the PWM voltage.

We are measuring the current using Current Probes on motor lines, and Power Supply Current Reading.

We are still investigating this. Rosario from ST also provided some more information about the current ratings at different configurations, and apparently, the Current Spec of the chip is about 1.7A in the "Dual Half Bridge" mode, which is the mode we are using. We probably overloaded the chip by 2 AMPs, and that is why it quickly burned.

Visitor II
November 11, 2025

Hi, did you ever end up figuring this issue out? I've had a few STSPIN958 burn down in our project too, it seems like thermal shutdown just never kicks in.