Skip to main content
Associate
August 15, 2024
Question

STSPIN958 EN Delay

Have a quick question. What is the delay time from when the EN is pulled high to when the half bridge becomes non Hi-Z? Similar is disable delay time from when the EN is pulled low? I wasn't able to find this information in the data sheet.

We will be operating in single half bridge (parallel) mode if that has any impact. Thanks!

This topic has been closed for replies.

1 reply

Cristiana SCARAMEL
ST Employee
November 12, 2024

Hello @twjudge and welcome to the ST Community.

Here below the typical value @ Tj = 25°C,
test conditions of Table 3 in the STSPIN958 datasheet, with "maximum slew rate" selected:

  • ENx high to power stage enabled propagation delay: 160 ns
  • ENx low to power stage enabled propagation delay: 240 ns

 

"If you feel a post has answered your question, please click ""Accept as Solution"""