Skip to main content
Associate
May 4, 2026
Solved

STSPIN840 Setting overcurrent values

Is the overcurrent protection set to 3A on the STSPIN840? If so, is there a way to change the trip value of the overcurrent protection to better align with its application? I want to change it so that the overcurrent trips at 1A. Thank you!

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 5, 2026

Welcome @mnguyen1, to the community!

The overcurrent protection is designed to protect the MOSFETs and has a fixed rating of typically 3A, max. 3.5A. The low-side shunts connected to SENSEA and SENSEB on each full bridge are used for the control and limiting functions.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 5, 2026

Welcome @mnguyen1, to the community!

The overcurrent protection is designed to protect the MOSFETs and has a fixed rating of typically 3A, max. 3.5A. The low-side shunts connected to SENSEA and SENSEB on each full bridge are used for the control and limiting functions.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mnguyen1Author
Associate
June 12, 2026

Thank you!

 

For the overcurrent protection, what’s the tolerance of when the circuit triggers. Say I have my Vref at 1V and my RSNSA is 0.5 ohms. I’m expected to trip at 2A, but could I expect to trip at 1.9? Thank you

 

Best,

Matthew

Peter BENSCH
ST Technical Moderator
June 17, 2026

See the answer to this 2nd question in your new thread.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.