Dear @Wzong.1
Sorry, I misunderstood your question.
PF6 and PF7 are not available on the pinout of the device, but they are internally connected to the gate driving circuitry.
In fact the STSPIN32F0 is a system-in-package embedding 2 silicon in the same package:
STM32F031 MCU + three-phase gate driver
The PF6 and PF7 of the STM32F031 are internally connected to the gate driver silicon.
For setting the OC values according to the table you just need to set the GPIOs through the code.
For example, the 100 mV threshold is set as following:
HAL_GPIO_WritePin(GPIOF,GPIO_PIN_6,GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOF,GPIO_PIN_7,GPIO_PIN_SET);