Skip to main content
Pavel Krupets
Associate III
November 16, 2018
Question

STSPIN250's can I use 3.3V for it's logic pins?

  • November 16, 2018
  • 0 replies
  • 475 views

STSPIN250's EN\FAULT and STBY\RESET pins are described as "Logic input 5 V compliant". Does it mean it only supports 5V logic or 3.3V logic will do the job of bringing these pins high?

Want to use this device with STM32L496 MCU which is a 3.3 device.

This topic has been closed for replies.