STSPIN220 Microstepping
I currently am running a stepper motor with a STSPIN220. I wanted to configure the STSPIN220 into 1/8 step mode, but I cannot decipher what I need to do to configure the microcontroller to send out the proper command to set the STSPIN220 into 1/8 step mode. From all the datasheets/app notes I have read, there is multiple configuration inputs to configure the step resolution. For my example of 1/8 step, there are two possible configuration inputs. While the 1/256 step has four possible configuration inputs.
I would greatly appreciated someone's insight on how to work with these multiple configurations for step resolutions for the STSPIN220.