Skip to main content
Associate
December 11, 2025
Question

STPS5H100AF operating temperature?

Regarding the STPS5H100AF, the datasheet states that the storage temperature is -65 to 175°C, but there is no mention of the operating temperature.

What is the operating temperature?

3 replies

Peter BENSCH
ST Technical Moderator
December 12, 2025

Well, in addition to the storage temperature range, the data sheet of the STPS5H100AF also contains the maximum operating junction temperature = 175°C and the thermal resistance Rth(j-l) = 16K/W. The maximum operating temperature permissible for the respective design can be calculated from the actual cooling surface of the board, the resulting thermal resistance and the power loss that occurs.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ryo10Author
Associate
December 14, 2025

 What is the minimum operating temperature?

Peter BENSCH
ST Technical Moderator
December 15, 2025

The diode is specified for industrial applications with a lower limit of -40DEGC.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.