Skip to main content
TWarn.1
Visitor II
September 23, 2021
Question

STPMIC1 - Suggestions on PWRGOOD signal output

  • September 23, 2021
  • 0 replies
  • 490 views

Generally, most regulators have a PG or PWRGOOD output that can be used by the system to know when it's safe to start booting.

With the digital signals on the STPMIC1, are there ones that could be configured to serve this purpose?

If not, I was considering using one of the LDOs, setting it to my digital voltage value, and pulling up my PWRGOOD input via a pull-up resistor. Also, I would put it in the last rank so that I knew all other voltages had adequate time to be stable.

Please let me know if there are better ideas.

Thanks,

Tom

    This topic has been closed for replies.