Skip to main content
Witold Sowa
Visitor II
June 22, 2017
Question

STPM32/33/34 with shunt on load high side

  • June 22, 2017
  • 0 replies
  • 679 views
Posted on June 22, 2017 at 22:39

Can I connect STPM32 to high-side of a load? If I do so then the shunt probes will be on 230V and 229.9V potentials. That is not wrong yet as I will not connect current negative input (IIN1) to mains neutral. My concern is that current positive pin and voltage negative pin are 0.5mm apart. The first will be at 230V potential, the second on 0V. Any ideas how to approach that?

#stpm33 #stpm32 #stpm3x #high-side #stpm34
This topic has been closed for replies.