Skip to main content
Associate
December 1, 2024
Question

STP45N60DM2AG TO247-LL heatsink is anode or cathode or insulated ??

Hi STteam,

 

I have selected STP45N60DM2AG MOSFET which is  TO247-LL package heatsink base  is anode or cathode or insulated may i know  ??

 

it is not mentioned in the datasheet.

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
December 1, 2024

This is the package variant TO-220, where tab is always connected to the centre pin, in this case drain.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
December 1, 2024

Sorry for mentioning wrong part number previosuly ,

i am using STPS61170CWLY diode ,  TO247-LL package heatsink base  is anode or cathode or insulated may i know  ??

Peter BENSCH
ST Technical Moderator
December 2, 2024

The same statement as before applies to this double Schottky STPS61170CWLY : the centre pin is connected to the tab, because this is the result of the lead frame geometry. However, you can also check this again by carrying out a continuity measurement between the centre pin and the tab. If there is no mention of insulation in the data sheet, then there is no insulation inside the device.

I am sorry that this is not explicitly mentioned again in the data sheet.

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.