Skip to main content
SSUBA.1
Visitor II
July 16, 2025
Question

STP40NF20 Drain voltage oscillation issue

Hi,

   We have build a led driver circuit using STP40NF20 -- 2 nos in parallel, the issue i am facing oscillation issue in Drain pin (Vled ), So kindly support in this regards..

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
July 16, 2025

There is no information about your idea and the schematics so far.

As I can see, you control the MOSFETs separately via one opamp each, whereby the opamps each amplify linearly with a factor of 11. However, it is absolutely not a good idea to control LEDs linearly, because their light emission depends not only on the flowing current, but also on the specific LED chip and its temperature. In addition, you want to work with a input control voltage between 0...5V, but because of the VDD of +12V, only a maximum of 12V/11=~0...1.1V can be used, even less if it is not an R2R opamp.

As far as connecting the stages in parallel is concerned, this is not a good idea with either linear or PWM control. Instead, the MOSFETs should be connected directly in parallel.

It would probably be best if you explained exactly what you want to achieve so that suggestions can be made.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.