Skip to main content
DSudo.2
Associate III
June 20, 2025
Solved

STP16CPC26 SDO output stuck low

This is our first board design that uses the STP16CPC26. We have two chips daisy-chained together. The SDO output from the first chip never goes high. The SDO pin is definitely not shorted to ground or any other net, and is definitely connected to the SDI pin of the daisy-chained downstream chip. If the chip is properly powered, the SDI pin is held high, and clocks are applied to the CLK pin, is there any reason why the SDO pin would not go high?

This topic has been closed for replies.
DSudo.2
DSudo.2Best answer
Associate III
June 21, 2025

MHoll.2 solved the problem (thanks again!). The problem was that the MCU was powered by 3.3V and the LED driver by 5V. The MCU at 3.3V could not meet the input high voltage spec for the LED driver.

1 reply

DSudo.2
DSudo.2AuthorBest answer
Associate III
June 21, 2025

MHoll.2 solved the problem (thanks again!). The problem was that the MCU was powered by 3.3V and the LED driver by 5V. The MCU at 3.3V could not meet the input high voltage spec for the LED driver.