Skip to main content
TMorg.1
Visitor II
June 25, 2020
Question

STP08DP05 Current Variation in a single output

  • June 25, 2020
  • 0 replies
  • 493 views

Background

I'm using STP08DP05 to control the current (20mA) through some LEDs in my design.

I'm using these for illumination purposes while I take an image.

I'm finding some variation in the brightness of my image, and I think it might to do with slight variation in the LED current changing the brightness of the LEDs.

Question

The data sheet doesn't seem to suggest what the variation in output current is for a single output, should I expect it to vary between the min and max levels of the output current (19mA-21mA) over time?

This topic has been closed for replies.