Question
STM32 FOC PMSM SDKv3.0 : Driving different motors
Posted on March 22, 2012 at 02:32
Hi
I have several different motors that I would like to drive (one at a time) using the same hardware and firmware based on the STM32 FOC PMSM libraries. The motor selection is indicated to the processor with a DIP switch so that the software can determine which motor is connected. The motors have different stator inductances, resistances and voltage constants so I need to change the dependent parameters C1 to C6 of the STO object. Does anybody have any suggestions of how this can be achieved? Thank you, Nick