Associate
January 29, 2024
Question
STEVAL-WBC86TX - Transmitter restarting after EPT
- 2 replies
- 1041 views
Hi
Once I send an EPT from the receiver device, STEVAL-WBC86TX disables its output, but after a few seconds it restarts automatically, even disabling repinging on the registers.
The receiver device, once it sends the EPT command, it should shutdown itself and remain off. But what happens is that it reinitializes after a few seconds, as like the transmitter was starting transmitting again, waking the receiver device up.
I have tried to disable repings.
Viewing the chart, it can be seeing that the output voltage starts decreasing after the EPT command from the receiver. But as soon it gets 0 volts, it instantaneously rises to 5V again.
Is there a way to avoid the transmitter to return transmitting after the EPT?
Thanks