Skip to main content
Associate
October 29, 2025
Question

STEVAL-WBC86TX transmitter board locked — I²C reset not working

  • October 29, 2025
  • 7 replies
  • 684 views

Hello ST community,


I have two STEVAL-WBC86TX transmitter boards that appear to be locked. The boards still charge a phone when powered, but the I²C reset tool provided by ST cannot communicate with the main IC. I've tried FT260 recovery tool. 

 

YLiu327_0-1761717954216.png

 

 

I would like to know whether there is a recovery or reprogramming method.

 

Thank you for any guidance.

7 replies

Didier HERROUIN
ST Technical Moderator
October 30, 2025

Dear YLiu327,

You can try with the recover tool attached.

It should reset and erase the chipset, then you can use the GUI to re-load the config/patch files selection "empty" at connection.

 

 
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Didier HERROUIN
ST Technical Moderator
October 30, 2025

..

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
YLiu327Author
Associate
November 4, 2025

YLiu327_0-1762284599219.png

Hi, this is the recovery tool that I've tried. However, it gave the chip ID 0xFFFF. 

any other options? 

 

Because I can see that both R14 and R16 are lit. 

Didier HERROUIN
ST Technical Moderator
November 5, 2025

Dear YLiu327,

It could mean that you chipset is now blank.

When you try to connect the GUI, select "Empty" instead of Rx/Tx: If it is able to connect, then, you can program the chipset. If not, the FTDI chipset may be damaged and you should test an external USB-I2C converter (removing jumpers on P2 and connecting SCL, SDA and GND to this connector).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
YLiu327Author
Associate
November 12, 2025

YLiu327_0-1762903045809.jpeg    

YLiu327_2-1762908788095.png

 

YLiu327_1-1762908777332.png

 

Hi Didier, 

what we have currently for external USB-I2C converter is C232HM-DDHSL-0, I removed the jumpers on the P2 of the 86Tx. 

based on the led signal of R14 the connection is there, 

but the recovery tool could not find the connection, I tired to scan if there is an connection actually between the converter and 86tx, or if I can find the device on the address 0x61, but it pop up that it has many devices on every single address. which is very confusing. 

 

Do you recommend any particular external USB-I2C converter that is good for our case here?
currently we could not connect the GUI/recovery tool to both transmitters.

Didier HERROUIN
ST Technical Moderator
November 12, 2025

Dear YLiu327,

I don't think that the USB-I2C converter should be specific.

On the picture you sent, I am not sure to see the right connections:
- the jumper on P1 should be in the position "middle" if you use the USB-C a power supply input
- the wires from your external USB-I2C converter should be connected on the "right side" of P2 connector : GND, SDA and SCL (considering that your converter includes pull-ups).

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
YLiu327Author
Associate
November 12, 2025

Dear Didier,

YLiu327_0-1762986128651.jpeg

YLiu327_3-1762986160182.jpeg

YLiu327_4-1762986180987.png

 

1. yes I have confirmed that the jumper is connected to the power source, which is the case "middle" in your reply.

2. I have tried both sides of the P2 SCL, SDA and GND, only one side, as shown in pic, had the R14 led on,

but both sides showed exact same results when i tried to find the board at 0x61. 

 

it showed 117 devices being on all addresses, which makes me feel that the board is actually not connected to the i2C converter. 

 

 

 

--------------------------------------------------------------------------------------------------------------------------------

this is also the case of both transmitters. 

YLiu327_5-1762986802268.jpeg

YLiu327_6-1762986808008.jpeg