Skip to main content
Associate III
November 10, 2023
Solved

STEVAL-WBC86TX -> Bricked accidentally, any chance of recovery?

Hello,

So I recently received the dev board STEVAL-WBC86TX and was quite impressed with the features. Accidentally the wrong config ID was written to the board. Now I cannot connect to it again using the Windows utility.

The USB to I2C appears to be working normally, but there is an error in the log and the device never connects successfully in the GUI, thus, I cannot flash the original config and nvm patch files from the website, provided as STSW-WBC86FWBPP.

[TX]WBC86 connection ex: Wrong config id 0xDA06 and patch id 0x0000 for TX"

I thought I could edit WBC86.json.enc, which probably contains which ID and such... I'm guessing this is encrypted json.

Is there a way to hard reset this chip to restore connectivity to the dev board?

 

This topic has been closed for replies.
willzhouBest answer
ST Technical Moderator
June 16, 2024

@AnkhInnovationsLLC 

please use this link tool

Wireless Charging solution Wiki - STMicroelectronics Community

 

willzhou_0-1718525293795.png

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

21 replies

Associate III
June 26, 2024

Hi @willzhou you rock!!!

It worked perfectly.

 

Is a similar tool available for the wbc 86?

ST Technical Moderator
June 26, 2024

Glad it is working, it is suitable for all wireless charge devices, include wbc86, it will auto read chip id and erase all patch and cfg.

@AnkhInnovationsLLC 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
January 23, 2025

I tried with dongle and the procedure work well, unfortunately it is work only with I2C dongle, if I restore the I2C interface of EVB STEVAL-SWBC86TXA I'm not able to read the chip ID.

Best Regards

 

ST Technical Moderator
January 26, 2025

Hi

can you share tool picture, if it show can not read chip id, it means chip is broken and I2C can not work

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
January 29, 2025

Hi,
I sent you a pdf with my setup and the value of the registers I read.

Best Regards

Alessandro

Associate
February 10, 2025

Hi Will,

Do you have new? We have often the Chip ID register corrupted. 

 

Best Regards

Alessandro