Question
STEVAL-SPIN3201 and MATLAB/SIMULINK
Hi,
[1] Is this board supported for automatic code generation in MATLAB/SIMULINK ?
[2] How high must the electrical rotary field resolution be for FOC operation, if I want to operate the PMSM without an observer?
[3] Is it possible to switch the operating mode BLDC (Hall sensors or BEMF) and FOC (encoder or observer) without board configuration ? Or do I generally have to change the firmware and hardware of the board like X_NUCLEO-IHM08M1 ?
Best Regards
Aaron