Skip to main content
oleg_sidorovich_1981
Associate III
Sep 29, 2020 1:01 PM UTC
Solved

Steval -SPIN3201

Can I connect oscillograph to Steval -SPIN3201 for measurement currents of the phase? Where is this point on board?

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Sep 30, 2020 6:28 AM UTC

Yes, of course.

Please take a look at the circuit diagrams and the UM2154 user manual of the STEVAL-SPIN3201. Perhaps you will find the shunt connections SENSE1P, SENSE2P and SENSE3P, which are amplified and then fed into the control at PA3/4/5. And if you then look at the board, you will find these test pads with a metal ring and the label PA3/4/5 around the controller.

Does it answer your question?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Sep 30, 2020 6:28 AM UTC

Yes, of course.

Please take a look at the circuit diagrams and the UM2154 user manual of the STEVAL-SPIN3201. Perhaps you will find the shunt connections SENSE1P, SENSE2P and SENSE3P, which are amplified and then fed into the control at PA3/4/5. And if you then look at the board, you will find these test pads with a metal ring and the label PA3/4/5 around the controller.

Does it answer your question?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
oleg_sidorovich_1981
Associate III
Sep 30, 2020 5:43 PM UTC

How I can use STEVAL-SPIN3201 for BLDC with MotorControl Workbench? In MotorControl Workbench only two types motors? To choose SM PMSM?

Cristiana SCARAMEL
ST Employee
Oct 1, 2020 12:15 PM UTC

Hello @oleg_sidorovich_1981​ 

please if @Peter BENSCH​ answered your main question "Select as Best" his reply.

Moreover, to help the Community to easily find the answer to similar questions open a new topic with the second request.

"If you feel a post has answered your question, please click ""Accept as Solution"""