Skip to main content
Cooke.Ernest
Associate III
April 4, 2017
Question

STEVAL PCC009V2 & SPINFamily Evaluation Tool

  • April 4, 2017
  • 0 replies
  • 726 views
Posted on April 04, 2017 at 17:25

/********* This question is also asked at ''Power Management and Motor Control > Discussions'' 

*********/

Hi,

I am trying to use the STEVAL-PCC009V2 & EVAL6470H boards using the SPIN

Family Evaluation Tool (Version 3.2)

However when I try to connect to the board I get the following error:

0690X00000606dLQAQ.png

I have managed to locate the below hex file at the following location:

C:\Program Files (x86)\STMicroelectronics\SPINFamily Evaluation Tool 3.2\Firmware

0690X00000606fFQAQ.png

I have tried to download the hex file below onto the board using Keil uVision but I am getting the following error in the Build Output.

0690X00000606hAQAQ.png

It should be noted that I was able get older versions of the SPINFamily Evaluation Tool to work.

If anyone has any solutions to this problem or has a link to Version 3 of the Evaluation Tool I would greatly appreciate it.

Kind Regards,

Ernest Cooke

#powerstep01 #dspin-gui #pcc009v2-eval6470h-spinfamily #keil-uvision
This topic has been closed for replies.