Skip to main content
Visitor II
August 13, 2025
Question

STEVAL-ISV019V1 High Battery Current

Hello!

I am attempting to charge a 3.7 V Li-ion battery using the SPV1050 on the STEVAL-ISV019V1 evaluation board, but there is a current coming from the battery into VBATT which ranges from 400 uA to 1 mA.

The current remains even when no load is connected, and when a solar cell is connected to PV+. Additionally, the current remains when the battery is replaced with a 4 V voltage source in series with a 1 kOhm resistor.

After reviewing the datasheet of the SPV1050 and the evaluation board, no components draw anywhere near this current so I suspect that my chip is damaged. However, the control logic and MPPT mechanism works perfectly fine so I am confused.

I'd be very grateful if anyone could help!

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
September 3, 2025

Welcome @mgrzybek05, to the community!

I don't have the STEVAL-ISV019V1 in front of me right now, so I can't check, but depending on the battery voltage (keyword: under-voltage protection), it is possible that the integrated pass transistor between STORE and BATT is closed and a small current flows from the battery into the device.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.