Skip to main content
JDupr.2
Visitor II
Sep 9, 2020 10:34 PM UTC
Question

STEVAL-ISB68WA not working with standard Qi transmitters

"...it works out of the box when placed on a suitable wireless power transmitter." is what it says on page 1 of the user manual. I have several Qi compatible transmitter pads, and the STEVAL-ISB68WA does not power-up with any of them. (D3 does not illuminate and no power is available at the output.)

Is there configuration required to get the STEVAL-ISB68WA to work with a standard Qi charger?

Joe

This topic has been closed for replies.

2 replies

TBurc.1
Visitor II
Jan 13, 2021 2:41 PM UTC

STEVAL-ISB68WA not working with standard Qi transmitters

I do have the same issue with the STEVAL-ISB68WA.

Could someone recommend a suitable wireless power transmitter that works with the EVAL Board?

BR Tom

HKhan.3
Visitor II
Aug 10, 2022 11:04 PM UTC

Was there a list of compatible Qi chargers?

Hash