Skip to main content
V.Gomez
Visitor II
Jan 4, 2023 2:15 PM UTC
Question

STEVAL-ISB68WA does not work with a commercially available 5W Qi compatible transmitter. Is this normal?

Hi,

I am working on a wireless power receiver test board 2,5W STEVAL-ISB68WA to develop an application with wireless charging.

STEVAL-ISB68WA does not detect a commercially available 5W Qi compatible transmitter (this one works properly).

According to “Getting started with STEVAL-ISB68WA wireless power receiver evaluation kit for wearable applications�? (see picture2), “The transmitter must be configured to have a ping frequency of 120 kHz and a 130 kHz -170 kHz operating frequency range�?.

Could you please tell me why the test board does not detect the transmitter?

Is this due to the transmitter ping frequency of 159.2 kHz (see picture1)?

Regards

GValere

    This topic has been closed for replies.