Skip to main content
Visitor II
January 22, 2026
Solved

STEVAL-IME014V1B

Hi,

I would like to use the evaluation board STEVAL-IME014V1B to drive piezoelectric transducers for medical applications. Does the evaluation module include a built-in H-bridge for direct drive of ultrasound transducers? May I directly connect the demo board to the transducers?

Regards

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
January 22, 2026

Welcome @Vx2026, to the community!

The STEVAL-IME014V1B is based on the STHV1600, which can directly drive 16 transducers.

However, no one here in the community can support either of these options because information about STHV1600 is only available under NDA from your local distributor or ST office.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
January 22, 2026

Welcome @Vx2026, to the community!

The STEVAL-IME014V1B is based on the STHV1600, which can directly drive 16 transducers.

However, no one here in the community can support either of these options because information about STHV1600 is only available under NDA from your local distributor or ST office.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.