Skip to main content
CC.1
Visitor II
December 12, 2019
Question

STEVAL-IHM023V3 in "3-phase HV FOC control for SMPMSM". We plan to use external control with 5V digital signals for all inputs (E-stop, PWM-H,L, brake, etc), It is save to set the Vdd at 5V in that case?

  • December 12, 2019
  • 0 replies
  • 477 views

We're planning to develop some motor drive academic boards for SMPMSM FOC motors for Master Students and for one of the parts we're using is STEVAL-IHM023V3. We're currently development the platform.

In the manual UM1823, page 28, table 6 for FOC control of HV PMSM 3-shunt, you state that if the 3-shunt configuration is to be used, the W1 jumper must be set to 3.3V.

That jumper is the one used for the vdd_micro value.

We will use independent external current measurement probes (isolated) and a non a STM control to attack the drive (externally powered).

Our inital questions is:

1) We plan to use external control with 5V digital signals for all inputs (E-stop, PWM-H,L, brake, etc), It is save to set the Vdd at 5V in that case?

This topic has been closed for replies.