Skip to main content
srinath mallikarjunan
Associate II
Jul 6, 2018 9:51 AM UTC
Question

steval-esc001v1 not detected

Posted on July 06, 2018 at 11:51

Hi

I try to connect to the board using STLink-v2 using IAR. But i get an error that device is not connected.

Board is powered from a 12V source. 

PWM lines are unconnected.

What could be the problem ?

#steval-esc001v1
This topic has been closed for replies.

2 replies

kyrreaa
Associate III
Jul 10, 2018 1:20 PM UTC
Posted on July 10, 2018 at 15:20

I've also had this problem until I found my connector pinning was reversed.

Check your pinnings again and again. You never know until you check twice.

srinath mallikarjunan
Associate II
Jul 11, 2018 11:35 AM UTC
Posted on July 11, 2018 at 13:35

Yes that was it..

I wish the picture they provide in the PDF was clearer.