Skip to main content
Visitor II
February 10, 2025
Question

STEVAL-DPSTPFC1 Hardware Problem

Hello.When I measure between 5V_SCR1 and GND_SCR2 in STEVAL-DPSTPFC1 Hardware, I see 9V. And when I start via Switch, it goes into standby mode when the output is unloaded and reaches 300V. It never becomes 400V. I quickly turn the switch to the off position again. I quickly turn it back to the on position. This time, all the LEDs go off. Can you please tell the technical team where the error and problem may be?

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
March 2, 2025

Welcome @BerkMaviengin, to the community!

Is there a special reason why you measure between 5V_SCR1 and GND_SCR2, which have nothing to do with each other? GND_SCR1 belongs to 5V_SCR1?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.