Skip to main content
Visitor II
May 10, 2024
Question

Stepper motor moves when touched

I'm currently controlling a closed loop stepper motor with an Arduino Uno R3 via the CL86 stepper motor driver. I also connected 2 buttons with pull-down resistors with which I can, for example, rotate the stepper motor by 90 degrees in one direction.

The control works so far, but the buttons also trigger when I touch their cables (e.g. the pull-down resistor) and also the stepper motor (metallic surface).

Why is that the case? Anyone have a tip?

This topic has been closed for replies.

2 replies

AScha.3
Super User
May 10, 2024

Missing ground /earth . So you should care for some ESD/antistatic area, but at least connect circuit ground to mains ground /earth .

And check your supply for correct insulation or let it check by someone, how knows about safety regulations and has the equipment to do a check.

Show a pic, what you have there, including supply.

If you feel a post has answered your question, please click on " Best Answer ".
Senior III
June 8, 2024

Make sure that you have connected uno gnd to the drive logical gnd . Try to reduce the button pull down resistor values. 

"If you feel a post has answered your question, please click ""Accept as Solution""."