Welcome @OTwin38BoH, to the community!
I am sorry that the formula in the data sheet, section 6.3, might be somewhat misleading. In the formula, the resistances are calculated in kohms, the voltage in volts and the current (the 20) in mA. In addition, there is no bracket around 20 - Rb(min), so VIN/20 must be calculated first.
For your values:
- VIN = 12V
- Rb = 95ohms = 0.095kohms
this results in (I have put a bracket around the division for clarity):
Rbleed = (12V/20mA) - 0.095kohms = 0.6kohms - 0.095kohms = 0.515kohms or 515ohms
Does it answer your question?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.