Skip to main content
Radoslaw Gembarowski
Visitor II
June 1, 2018
Question

Stc3117, ocv reg when vbat is lower when ocv table

  • June 1, 2018
  • 0 replies
  • 424 views
Posted on June 01, 2018 at 11:40

Hi,

I am using the battery monitor - stc3117.  The application uses the default OCV table.  When the battery monitor is initializated,  vbat is set to 3V (on the battery simulator), but Ocv register is  3.3V. It is the lowest value in the OCV table.  Is it  proper  behaviour of the monitor ?

Regards,

RG

#stc3117
This topic has been closed for replies.