Skip to main content
Chip Weller
Associate
January 29, 2018
Question

STC3115 Adjusting Configuration

  • January 29, 2018
  • 0 replies
  • 600 views
Posted on January 30, 2018 at 00:22

After reading the STC3115 datasheet (D023755 Rev 8) and system integration (AN4324), plus FAQ and the driver code on GitHub, I have questions about the REG_VM_CFG, REG_CC_CFG, REG_VM_ADJ and REG_CC_ADJ.

Are the *_CFG parameters automatically updated by the IC?

If not, is there an algorithm I should used to adjust them with the *_ADJ registers?

Thanks

#stc3115
This topic has been closed for replies.