Skip to main content
Associate
June 24, 2025
Solved

STC3100 Current register nonsense values

Hi, 

I am having the same issue as this previous forum post, but the question was never answered. 

 

Voltage and temperature sense give expected readings. 

REG_VOLTAGE_LOW: 29; REG_VOLTAGE_HIGH:6 --- VOLTAGE: 3818mV

REG_TEMPERATURE_LOW: 186; REG_TEMPERATURE_HIGH:0 --- TEMP: 23 deg

 

from the datasheet ---> current (mA) = current_code* 11.77 / Rsense (mΩ)

REG_CURRENT_LOW: 203; REG_CURRENT_HIGH: 54 --- CURRENT: 15429mV

Where the actual current for my application is 2.5A. I am using a 10mOhm current sense resistor. Indeed a multimeter reveals 25mV drop across it. 

 

Could somebody please tell me if this is a hardware issue? I have followed all recommendations in the datasheet closely, but cannot find a reason that current is this high. Furthermore, when my application draws only 3.5mA, the current reads 18018mA

 

Thank you very much. 

 

 

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
July 3, 2025

I noticed something else besides the missing type casting mentioned before:

Your example values are probably due to negative currents, i.e. current from the cell towards the load, right?
Let's take your values of REG_CURRENT:

  • Low=203; High=54, i.e. 0x36CB
  • according to the data sheet, section 6.1.4 the value is represented in two's complement (of 14-bit), which results for your values in a negative 0x16CB
  • 0x16CB * 5.88µV/LSB = 34.3098mV

This value is much closer to the 25mV you measured externally, isn't it?

However, I am also not sure that the 5.88µV in the data sheet is correct: the measuring range of the STC3117 is ±40mV, which corresponds to a resolution of 4.88µV at 14-bit (16384 steps). With these 4.88µV we would arrive at 28.4748mV.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

Peter BENSCH
ST Technical Moderator
June 24, 2025

Welcome @rs231, to the community!

If the maximum current to be measured is 2.5A, you should use a shunt of 80mV/2.5A = 32mohms, maybe only 30mohms to have some margin at the top.

Can you insert some schematics as a picture and please also the part of the programme that reads out the STC3100 so that both can be checked?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
rs231Author
Associate
June 25, 2025

Hi Peter, 

Thanks for getting back to be quickly!

I noticed that the max voltage is +/- 80mV. Since 2.5A corresponds to 25mV with the 10mOhm shunt, I thought this should be alright? 

I will post the code for the working temperature, vs the non-working current. Note unsigned integers are used for now but both values are positive. The environment is C in Zephyr RTOS. 

 

void read_current(void)
{
 uint8_t buf[2] = {0};

 int ret = i2c_burst_read_dt(&i2c_fuel_gauge, REG_CURRENT_LOW, buf, 2);
 if (ret == 0)
 {
 printk("raw current lower: %d\n", buf[0]);
 printk("raw current upper: %d\n", buf[1]);

 uint16_t raw_current = (buf[1] << 8) | buf[0];
 printk("raw current total: %d\n", raw_current);

 int current_mA = raw_current * (1177 / 100) / SENSE_RESISTOR_MILLI_OHMS;
 printk("current_mA: %d mA\n", current_mA);

 }
 else
 {
 printk("Failed to read battery current: %d\n", ret);
 }
}

 

void read_temp(void)
{
 uint8_t buf[2] = {0};
 int ret = i2c_burst_read_dt(&i2c_fuel_gauge, REG_TEMPERATURE_LOW, buf, 2);
 if (ret == 0)
 {
 printk("raw temp lower: %d\n", buf[0]);
 printk("raw temp upper: %d\n", buf[1]);

 uint16_t raw_temp = (buf[1] << 8) | buf[0];

 int temp_deg = raw_temp * 125 / 1000;
 printk("Fuel Gauge temp %d deg\n", temp_deg);
 }
 else
 {
 printk("Failed to read fuel gauge temp: %d\n", ret);
 }
}

 

The schematic is as follows: 

rs231_0-1750818474441.png

rs231_1-1750818492334.png

 

 

Thanks for your help.