Skip to main content
rvalascho
Associate II
September 29, 2003
Question

startup issues

  • September 29, 2003
  • 2 replies
  • 800 views
Posted on September 29, 2003 at 11:24

startup issues

This topic has been closed for replies.

2 replies

rvalascho
rvalaschoAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 10:16

I am having trouble starting our motor due to high inertia. The current is maxed out for starting torque, are there any other solutions?

Now I have a 300 Volt control with a higher resistance and higher inductance, and it will start fine with high inertia.

My 24 V control, which is my problem, has lower resistance and inductance. How would this effect startup if essentially I put the 300 Volt code into the 24 Volt?
rvalascho
rvalaschoAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 10:16

When I refer to higher impedance and inductance, I am referring to the motors in which the control is connected.