Skip to main content
lbug.1
Visitor II
Jul 25, 2022 1:16 PM UTC
Question

ST1S14PHR power instability

I'm using ST1S14PHR like the attached schematic, but with an input between about 10V and 20V the output is instable and appears 2.8/3.2V ...sometimes after a few seconds the stable situation at 5V is reached.

After the ST1S there is a linear 3v3 regulator that with the instable input has an instable output.

Absorption at 24V is about 30mA.

What could be the problem?

thanks...

    This topic has been closed for replies.