Skip to main content
Guille
Associate II
September 3, 2025
Solved

ST1PS02 - Impedance of logic inputs D0 D1 D2

Regarding ST1PS02. Which is current drained from logic inputs D0 D1 D2 when connected to Vin?
Is it safe to pullup them to VOUT, i.e., can it cause startup issues?
Thanks for the attention.

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
September 4, 2025

D0, D1 and D2 are high impedance logic inputs, so their input current is generally negligible and should be in the order of nanoamperes.

The same maximum voltage is specified for D0, D1 and D2 as for VIN. Since this is a buck regulator, you can also connect D0, D1 and D2 to VOUT.

Does this answer your questions?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
September 4, 2025

D0, D1 and D2 are high impedance logic inputs, so their input current is generally negligible and should be in the order of nanoamperes.

The same maximum voltage is specified for D0, D1 and D2 as for VIN. Since this is a buck regulator, you can also connect D0, D1 and D2 to VOUT.

Does this answer your questions?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Guille
GuilleAuthor
Associate II
September 26, 2025

Thanks for your response Peter.
My question about connecting pull ups to Vo was because at startup, when the IC is powered, Vo is initally 0, so I was not sure that in the transient phase, when Vo is rising, things actually go as it should do, i.e. pull ups seeing the right voltage value. Also because the output value itself depends directly on those pull ups.
Thanks for the attention.

G.F. 

Peter BENSCH
ST Technical Moderator
September 26, 2025

Ah, now I understand the background to your question. I can reassure you that the pull-ups at the inputs read the correct logic value even when switching on.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.