Question
ST Motor Control Workbench "PDSC version is not supported"
- 4 replies
- 3132 views
Hi, I am currently working on a project that uses a BLDC motor (42BL90L2-3), and I am trying to drive it using a DRV8323 gate driver. I have been using the ST MC workbench (version 5.4.8) to profile the motor and control unit, but when I try to generate the project I get a whole bunch of errors stating "PDSC version is not supported". The project still generates, but after importing it to CubeIDE it will always HardFault when I try to debug, it never makes it to the while() loop. I am using CubeMX version 6.2.1 and STM32 FW V1.8.4. Has anyone else ever encountered this issue?