Question
SPV1050 very bad efficiency with solar panel. In same condition charge current is 15mA with spv1050 and 50mA with battery directly connect to solar panel. Help need
I use a solar panel ref SM141k08l from IXOLAR and the sp1050 schematic from eval board ISV020V1 in a buck boost version. Just change some resistor to adjust Vppm to 4.8v (I got it in my test, but only 15mA is push to my Lipo battery, lipo voltage is 3.8v and Veoc and Vuvp are correct).. I could share my schematic. I need help because I didn't understand what's happen. Emmanuel from GEO2I