Skip to main content
Visitor II
January 14, 2025
Question

SPV1050 Mode Issue

  • January 14, 2025
  • 1 reply
  • 639 views

I am designing a PV cell charging circuit with SPV1050.

When the configuration is set to boost mode, I am curious what happens if a voltage higher than Veoc is applied to the PV cell.

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
January 17, 2025

Well, the data sheet states in table 4, parameter VIN_LV for boost configuration a range of min VEN_TH and max VEOC. In addition, table 2 (absolute max ratings) mentions a value of VSTORE+0.3V for IN_LV. You must therefore ensure that this range is not exceeded.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.