Welcome @01Solutions, to the community!
There are several ways you can limit the charging current, which also depend on how your overall system is set up and where your load is connected:
- Limiting the SPV1050’s output power by limiting the input current
- Charge controller on BATT, e.g. with the L6924D or a discrete linear regulator
20mA at a maximum of 4.2V corresponds to a maximum charging power of 84mW. If your source stays below that plus the losses, the charging current should be automatically limited.
Hope that helps?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.