Skip to main content
Associate
October 15, 2025
Question

SPV1050 Charging Problem

Screenshot_47.png

Hello,

I designed a circuit, but there is a problem with it. My supercapacitor (C5) is charging very slowly. I am using Dracula's standard OPV. It receives an average of 500 lux. It is charging so slowly that it is almost not charging at all. What could be the problem?

Thank you.

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
October 15, 2025

Welcome @Bard48, to the community!

First, I would check the electrical parameters or characteristic curve of the OPV (organic voltaic cell), as we do not have this data for 500lx).

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Bard48Author
Associate
October 15, 2025

Thank you for your response.

OPV specifications: In 500 lux; Voc=3,67V, Isc=190uA, Vm=2,95V, Im=162mA, Pm=478uA

I can see that it charges very slightly. When I connect a 50mA load, the 3.3V LDO in the system disables. As far as I understand, even though my supercapacitor has sufficient charge, the Internal Pass Transistor disconnects the connection.

What could be the problem?

Thank you.

 

Peter BENSCH
ST Technical Moderator
October 15, 2025

Pm=478μΑ?!

To me, P stands for power, right?

Are you able to measure the voltage and current out of the OPV using an ohmic resistor?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.